Technical FAQs

Ask a Question

What are the specifications of Enerpact thermal and static ACB internal current transformers.

The Enerpact thermal and static ACBs have wound current transformers.

> CTs for Thermal Enerpact ACB
Rated current/5A
3VA, Class 5P6
S/C withstand 80ka for 1 Sec.

> CTs for Static Enerpact ACB
Rated current/5A/50mA (Double winding)
5A - 2VA, Class 5P8
50mA - 0.75 VA, Class 5P8
S/C withstand 80ka for 1 Sec.

 
Was this helpful?
What can we do to improve the information ?