Technical FAQs

Ask a Question

What is the Coating material of rear connection for Masterpact NW.

The terminal connections coating on Masterpact are the following :

1) Rear connection for NW08 to NW20 and front connection for NW08 to NW16: aluminium tin plated

2) Rear and front connection for NW25 to 63 : copper with silver plated
Was this helpful?
What can we do to improve the information ?