Technical FAQs

Ask a Question

Can the ATV212 drive operate in FIRE mode bypassing the fault.

With the Function 52 'Forced mode' the drive will run until drive breaking (overcurrent, overvoltage, ... can not stop the drive), stop button does not stop the drive.
With function 53 'Fir mode' the drive run but in critical fault, stop the drive and the STOP button of the front panel stop the motor too.
Was this helpful?
What can we do to improve the information ?