Technical FAQs

Ask a Question

What is the thermal current(Ith) and operational current (AC3) of GV2*32

Thermal current and operational current values are provided below

- Thermal current Ith equal to thermal setting current and value is 32A

- Operational current for GV2*32 is from 24 to 30A in AC3 category.

Was this helpful?
What can we do to improve the information ?