Technical FAQs

Ask a Question

What is rating of changeover contact 33751, 33752 and 33753 of Masterpact NW at 240V AC and 250V DC

Rating of changeover contact of Masterpact NW 33751, 33752 and 33753 is given below

a. At 240V AC, 380V AC, 480V AC is 8A
b. At 250V DC is 0.3.

Was this helpful?
What can we do to improve the information ?