Technical FAQs

Ask a Question

Is it possible to generate pulse once 100 kwh in MERSEPM5100 which has no communication ports.


No, It is not possible to generate pulse once 100kwh. 

No of pulse can be changed from 1 to 9999999 but pulse generated by meter will be for 1 kwh only. 

1 kwh cannot be changed to 100 kwh in meter. 1 kwh setting is standard feature of meter. 
 
Was this helpful?
What can we do to improve the information ?