Technical FAQs

Ask a Question

What is the advantage of using M2C test adapter when doing secondary injection test on Masterpact Breaker.

Main function is using M2C Test Adapter is that When using the M2CTEST special adapter, all advanced protections, logging of trips, logging of alarms, activation of alarms and
incrementing of the contact wear counter are enabled during the secondary injection test.

But when you test directly using FFTk, logging of alarms, activation of alarms and incrementing of the contact wear counter are enabled during the secondary injection test are disabled

This is the main advantage of M2Ctest Adapter.

All protection would be available with M2CTest Adapter that includes Ig as well.
Was this helpful?
What can we do to improve the information ?