Technical FAQs

Ask a Question

What is the Shock test specification iEM3210

Shock test specification of iEM3210 is provided below:

1. Impulse Wave Type : Half Sine Wave
2. Peak acceleration : 30g
3. Duration          : 18ms
4. Pulse Cycles      : 3
 
Was this helpful?
What can we do to improve the information ?