Technical FAQs

Ask a Question

What is the Shock test specification PM3250


Shock test specification of PM3250 is provided below:

1. Impulse Wave Type : Half Sine Wave
2. Peak acceleration : 30g
3. Duration          : 18ms
4. Pulse Cycles      : 3
Was this helpful?
What can we do to improve the information ?