Technical FAQs

Ask a Question

What is the air flow detail for ATV310 drives.

ATV310HU15N4: 14 m3/hour
ATV310HU22N4: 14 m3/hour
ATV310HU30N4: 30 m3/hour
ATV310HU40N4: 30 m3/hour
ATV310HU55N4: 30 m3/hour
ATV310HU75N4: 60 m3/hour
ATV310HD11N4: 60 m3/hour
Was this helpful?
What can we do to improve the information ?