Technical FAQs

Ask a Question

Is TSXPBY10 is profibus slave module? And how it is related with TSXPBY100 ?

No, The TSX PBY 10 module is a PROFIBUS-DP master communication module.

The TSXPBY100 = TSXPBY10 + PCMCIA

A PBY100 is a ''package'' that includes a PBY10 module + a PCMCIA card

The module is labeled PBY100 on the top front face and the sticker on the side is a PBY10.

The part numbers TSXPBY10 and TSXPBY100 are kits pertaining to Profibus network. Both kits includes the the following:
1. TSXPBY100 host module
1. PCMCIA card with cable
3. T junction box 
Was this helpful?
What can we do to improve the information ?