Technical FAQs

Ask a Question

What are the consequences of STBNIP2311 master controller setting.

The STBNIP2311 module can be configured to recognize up to three controllers as master controllers. The module should continuously maintain an open connection with at least one master controller. 
If the STBNIP2311 module loses all connections with master controllers: -
  • It waits a prescribed time (Holdup Time) for a master controller to establish a new connection with the STBNIP2311 module. 
  • If no new connection is established before the timeout period expires, the STBNIP2311 module sets island outputs to their fallback states.
Was this helpful?
What can we do to improve the information ?