Technical FAQs

Ask a Question

What is Sensor Alignment for M340 Analog modules and how it categorized for Filtering.

Sensor Alignment is the process of "alignment" consists in eliminating a systematic offset observed with a given sensor, around a specific operating point. This operation compensates for an error linked to the process. Replacing a module does not therefore require a new alignment. However, replacing the sensor or changing the sensor's operating point does require a new alignment.

Alignment filtering is being categorized as below:

0  = No filtering 

1 or 2 =  Low filtering 

3 or 4 = Medium filtering

5 or 6 = High filtering

NOTE: To align several analog channels on the BMX ART/AMO/AMI/AMM modules, we recommend proceeding channel by channel. Test each channel after alignment before moving to the next channel in order to apply the parameters correctly. 
Was this helpful?
What can we do to improve the information ?