Technical FAQs

Ask a Question

Can the coil A1-A2 and E1-A2 of CR1F supplied continuously

A1-A2 and E1-A2 coil of CR1F cannot be supplied continuously. In the coil , there is  an internal NC contact , when switch is on ON position, the moving part of the contactor will open the internal NC contact. 
For opening , we use the auxiliary contact 13-14 in series. 
Was this helpful?
What can we do to improve the information ?