Technical FAQs

Ask a Question

What is the scaling range of parameter Estimated motor current on AO1 assignment for ATV310 drive.

The scaling range of parameter Estimated motor current on AO1 assignment for ATV310 drive is 0~2*In(rated drive current).
 
Was this helpful?
What can we do to improve the information ?