Technical FAQs

Ask a Question

Is possible to connect the breaking resistor between PA/+ and PB and also need to used DC chokes (PO and PA/+) on ATV71 drive.

Yes, it is possible to connect the breaking resistor between PA/+ and PB and also
It is possible to connect DC chokes (PO and PA/+) on ATV71 drive.
 
Was this helpful?
What can we do to improve the information ?