Technical FAQs

Ask a Question

What is the parameter of second ramp switching & how it works on ATV312 drive.

Example:
ACC=5 & dEC=5
If rPS(ramp switching assignment) is assigned to LI3.
 
And Frt([Ramp 2 threshold] is 20 Hz.
The 2nd ramp is switched if [Ramp 2 threshold]] (Frt) is not 0 (the value 0 corresponds to the inactive
function) and the output frequency is higher than [Ramp 2 threshold]] (Frt).
 
And AC2 =10, dE2=10.
 
Explanation:
If LI3 is OFF and output frequency is less then Frt (i.e.20 Hz) then drive will follow ACC & dEC
If LI3 is OFF and output frequency is greater then Frt (i.e.20 Hz) then drive will follow AC2 & dE2
If LI3 is ON and output frequency is less then Frt (i.e.20 Hz) then drive will follow AC2 & dE2
If LI3 is ON and output frequency is greater then Frt (i.e.20 Hz) then drive will follow AC2 & dE2
 
Note: AC2 and dE2 is depends on Frt and LI3 (ON & OFF).
 
Was this helpful?
What can we do to improve the information ?