Technical FAQs

Ask a Question

What is the scaling range of parameter Motor thermal state and Drive thermal state on AO1 assignment for ATV310 drive.

The scaling range of parameter Motor thermal state (THR) and Drive thermal state (THD) on AO1 assignment for ATV310 drive is 0% to 200%.
Was this helpful?
What can we do to improve the information ?