Technical FAQs

Ask a Question

What is the part number of 3 way selector switch with 2 number NC contact and padlock at center.


Part number of 3 way selector switch with 2 number NC contact and padlock at center : ZB4BJ593+ ZB4BZ104
 
Where ZB4BJ593 is black selector switch head Ø22 3-position spring return to centre, Black long handle and Padlockable at center only.
 
ZB4BZ104 is complete body/contact assembly with 2NC.
 
Refer to attachment for the data sheet of ZB4BJ593 & ZB4BZ104.
 
Was this helpful?
What can we do to improve the information ?