Technical FAQs

Ask a Question

What are the power quality standards for which PM8000 comply.

The PM8000 includes the following power quality compliance:

• EN50160: The meter measures and presents statistics for determining EN50160
compliance.
• IEC 61000-4-30: The meter complies with the IEC 61000-4-30 power quality
standard.
• IEC 62586-1: The meter complies with the IEC 62586-1 power quality standard.
Was this helpful?
What can we do to improve the information ?