Technical FAQs

Ask a Question

What are the main features of Com'X 510.

The main features of the Com'X 510 are:
  • real-time data in easy to understand views.
  • dashboard view for historical reporting.
  • automatic discovery of connected Modbus devices connectivity to the cloud through three media: GPRS, wired Ethernet, or Wi-Fi Ethernet.
  • two Ethernet ports to separate upstream cloud connection from field device network.
  • four supported transfer protocols: HTTP, HTTPS, FTP, and SMTP with proxy management.
  • data logging.
  • data export with native connection to Schneider Electric service platforms (such as Energy Operation) and with .csv file for other database servers.
  • gateway functionality Modbus TCP to Modbus RTU or Modbus ASCII.
  • setup through on-board web pages.
  • compliant with electrical switchboard environment (temperature, electromagnetic compatibility).
  • local backup of configuration parameters.
  • ZigBee Pro with EM4300 sensors.
Was this helpful?
What can we do to improve the information ?