Technical FAQs

Ask a Question

Why we are not able to Launch the Hardware Catalog Manager for Unity Pro Software.

NOTE: Hardware Catalog Manager and Unity Pro software cannot both be running at the same time.

Below shows the procedure to launch the Hardware Catalog Manager :

1.  Verify that Unity Pro software is not running
  • if Unity Pro Software is running, close it
  • if Unity Pro Software is not running, go to the next step  
2.  Select:
Start → Programs → Schneider Electric → SoCollaborative → Unity Pro → Hardware Catalog Manager
Was this helpful?
What can we do to improve the information ?