Technical FAQs

Ask a Question

Can I connect a PC to a remote I/O module port in EIO System.

Yes, but PCs will not be able to communicate with any modules. We recommend you connect PCs (or any other non-remote I/O device) to the following:
  • a 140 CRP 312 00 module — DIO Cloud or DIO Sub Ring port
  • a 140 CRP 312 00 module — INTERLINK port or SERVICE port configured as an access port
  • a ••• CRA 312 •0 adapter module — SERVICE port configured as an access port
NOTE: Do not connect a device with a speed in excess of 100 Mbps to the SERVICE port. If the device is configured for a speed that exceeds 100 Mbps, the Ethernet link may not be established between the device and the module through the SERVICE port. 
Was this helpful?
What can we do to improve the information ?