Technical FAQs

Ask a Question

Is it possible to add custom Model in Comx510.

The Com'X 510 supports the use of custom models. A custom model is any model other than
a Built-in model from Schneider Electric. To use a custom model, you must first create a new
custom model. A custom model can be:

1. based on a previously created custom model
2. an entirely new model

For complete procedure refer attached file.
Was this helpful?
What can we do to improve the information ?