Technical FAQs

Ask a Question

What impact would THDi of 35% have on the over voltage and under voltage protection on the P and H control unit

The breakers are intended to work propely when THDi < 10% and THDv < 5%.  

If THDi is most of the time over 10%, so this could cause nuisance tripping and overheating. So it is advice to add Harmonic filters.
 
Was this helpful?
What can we do to improve the information ?