Technical FAQs

Ask a Question

What is the inrush current of Electric Motor (MCH) of Masterpact NT/NW.

Power Consumption of Electric Motor MCH of masterpact NT/NW is 180VA. Depending upon the voltage rating of MCH, rated current is calculated using P = VI and the Inrush Current of Motor will be 2 to 3 In of rated current.

For Example , Motor rated Voltage is 240V and Power Consumption is 180 VA. So rated current would be 0.75 A using P=VI. So the Inrush current would be 1.5 to 2.25A for 0.1 second.

 
Was this helpful?
What can we do to improve the information ?