Technical FAQs

Ask a Question

Is SLS features concerning to safety available on ATV32 drive.

ATV32 has better features concerning to safety - it can perform:
- STO (Safe Torque Off, stopping category 0 and 1)
- SS1 (Safe Stop 1),
- SLS (Safely-Limited Speed).
 
Was this helpful?
What can we do to improve the information ?