Technical FAQs

Ask a Question

Is it possible to use SST function of ATS48 on application.

SST (Tests on small motor) function is made only to test (in labs only.)
In this mode a lot of functions are not active (no current-torque control, no protection ...etc….).
So, it is not recommended to use SST function for applications.
 
Note:
• SSt returns to the OFF state as soon as the control voltage is disconnected.
• SST is only dedicated for maintenance and testing of the starter.
 
Was this helpful?
What can we do to improve the information ?