Technical FAQs

Ask a Question

What is the difference between XACA482 and XACA481.

The reference XACA482 is only sold under reference XACA482H50.
Both references XACA481 and XACA482H50 are based on the same XACA 4 holes but the functions are completely different: Please refer to attachments.
Was this helpful?
What can we do to improve the information ?