Technical FAQs

Ask a Question

In case of damage of ATV Process drive, is it possible to recover parameter data from PLC for VSD replacement easily.

There is the function FDR (Fast Device Replacement), The FDR service is used to simplify the maintenance of drives connected on the Ethernet network. In the event of drive not functioning correctly, this service automatically reconfigures its replacement.
 (refer to attached manual page 56 for ATV Process). This function is available for ATV32, ATV61, ATV71 and ATV Process with Ethernet / Modbus TCP. Be careful, the PLC must have the function server FTP.
Was this helpful?
What can we do to improve the information ?