Technical FAQs

Ask a Question

What is the specification of Sling(rope) which is used to mount ATS48 soft starter using DNV kit.

It is must to choose the material of Sling (rope) enough hardness for maintain the starter. Refer to installation manual, minimum force level is given on the Sling.
it is possible to use 0 to 14 mm thick rope depending on the weight of the soft starter. Find the view of sling in attachment.
Was this helpful?
What can we do to improve the information ?