Technical FAQs

Ask a Question

Is it possible to use motor greater than the ATV71 drive power.

 
The use of a motor with a higher power rating than that of the drive is only possible if the current drawn by this motor is less than or equal to the nominal drive current. Refer to catalog page in attachment.
 
Was this helpful?
What can we do to improve the information ?