Technical FAQs

Ask a Question

what is the operating range of onboard PM8000 digital Input.

The PM8000 digital inputs are not self-excited and require an external whetting source (available on digital expansion modules). The onboard digital inputs operate between 5Vdc and 60Vdc and draw about 1-3mA.
Was this helpful?
What can we do to improve the information ?