Technical FAQs

Ask a Question

What is Pulse output voltage of EM1000 Meter and is the Pulse width programmable.

Pulse output voltage of EM1000 is 24V DC and it is possible to programme Pulse Width from 50 to 500ms

Was this helpful?
What can we do to improve the information ?