Technical FAQs

Ask a Question

Getting 'CID File Validation Error' in Kernel and #BAD in Citect Runtime when communicating an IED on IEC61850 Protocol

A CID file is validated when the IEC61850 driver establishes a successful connection with a device. The file is validated using the following processes:

  • Variable attribute validation
  • Dataset validation

Add the following parameter to citect.ini configuration file:
[IEC61850N]
CIDFileValidationType=1
After adding above parameters, save, reload, compile and run the project.

Was this helpful?
What can we do to improve the information ?