Technical FAQs

Ask a Question

How to change the expired Password of HMI from Vijeo Designer Run Time.

When a user password expires, the operator must change the password. The method to change the password differs depending on the login method:

  • Logging in using a Login part, FixedNameLogin part, or script method "Sys.login" – On password expiry, after the operator logs in successfully, a new password panel opens indicating your password has expired and allows the operator to enter and confirm a new password.

  • Logging in from the Web Server/Web Gate, or using an Authorization Toolchest part or script method "Sys.validateUser" – On password expiry, the login will fail and a system message will display. The operator will need to log in using a Login part, FixedNameLogin part, or System Login Panel, and then will be able to change the password.

In the event the password has expired, the operator can still log in using the expired password and download to a panel using File System.

Was this helpful?
What can we do to improve the information ?