Technical FAQs

Ask a Question

What is the Compact NS 33722 Chassis Material.

The Compact NS 33722 has a cold rolled steel as per EN 10130-DC-A-m for chassis main material.
Was this helpful?
What can we do to improve the information ?