Technical FAQs

Ask a Question

How to add GSM Modem in Somachine Project

To add GSM modem in Somachine project use the following steps:

- Right click on serial line in Device Tree and select add device
- Select ASCII Manager from the protocol manager list
- Right click on ASCII Manager and select add device
- Select vendor name to Schneider Electric and select appropriate GSM Modem

GSM modem will be added in device tree. Refer the attached snapshot.
Was this helpful?
What can we do to improve the information ?