Technical FAQs

Ask a Question

Recommended wire size (AWG size) for I/O signal connection to M221/241/251 and TM3 Expansion module.

All the wiring recommendations are mentioned in  M221/241/251 and TM3 Expansion module hardware guides.
Kindly refer the attached wiring guidelines part from these hardware guide. 

 
Was this helpful?
What can we do to improve the information ?