Technical FAQs

Ask a Question

How to do Local access to the control console in PDPM144F ?

Follow the below steps :

For local access, use a computer that connects to the Modular PDU through the serial port, to access the
control console:
1. Select a serial port at the computer and disable any service that uses the port.
2. Connect the provided serial cable from the selected port on the computer to the configuration port
at the NMC.
3. Run a terminal program such as HyperTerminal, and configure the selected port for 9600 bps, 8
data bits, no parity, 1 stop bit, and no flow control.
4. Press ENTER, and at the prompts, enter your user name and password.
Was this helpful?
What can we do to improve the information ?