Technical FAQs

Ask a Question

How to Disable "STOP" button on keypad of ATV212 in the Remote mode

Warning : You are going to disable the stop button located on the drive and graphic display option.
                  Do not select / unless exterior stopping methods exist. 
                  We never recommend that you should disable the stop button on the drive
.


You can disable the stop key by navigating to parameter F734. Set this parameter to 1 [Disable].

Refer the attachment for more details.



 
Was this helpful?
What can we do to improve the information ?