Technical FAQs

Ask a Question

What is the function of "Zero Switch" in SPD310/SPD360 Sensor.

If  "Zero Switch" has been pressed and hold the for 2 seconds then the pressure differential will reset to zero. This needs to be performed when both positive or negative pipes are disconnected.
It should only be necessary to perform a reset if there is reason to believe that the analogue output signal is not as expected.

Please refer the attached instruction sheet.

 
Was this helpful?
What can we do to improve the information ?