Technical FAQs

Ask a Question

What will be the derating factor for LC1D with DC coil at 90 rotation position.

The Only derating when you turn 90°on a side a LC1D with DC coil is a reduction of possible switching per hour. 
You have to apply a ratio of 0,65 on this number so maximum operations per hour(For LC1D09-38) is 3600 x 0,65 = 2340.
 
Was this helpful?
What can we do to improve the information ?