Technical FAQs

Ask a Question

What will be the maximum permissible frame temperature of C60H-DC.

The C60 HDC MCB is complied with IEC-60947 standard. 

The max operating temperature is 70°C; that mean: 
-material of operating handle => 70+25 = 95°C 
-material of case and cover => 70+50 = 120°C 
-material of external connection terminal => 70+60 = 130°C
Was this helpful?
What can we do to improve the information ?