Technical FAQs

Ask a Question

Is the electrical durability Chart of the Tesys D contactor in AC3 category is the same for an IE3 motor as for other motors.

The electrical durability Chart of the Tesys D contactor in AC3 category is the same for an IE3 motor as for other motors.

In AC3, the wearing of the power contacts of a contactor occurs at breaking, not at making, even if the making exceeds 6 times the rating as it is the case with an IE3 motor.

Was this helpful?
What can we do to improve the information ?