Technical FAQs

Ask a Question

What is the communication response time over Ethernet for one to one communication with PM5560 meter to fetch 30 parameters ?

The communication response time through Ethernet mode when the meter and Modbus tool are in one to one connection, for 30 parameter is 3.5mS.
However the update time for all parameters in meter is 1 second.

 
Was this helpful?
What can we do to improve the information ?