Technical FAQs

Ask a Question

What are the programming parameters to run ATV630 drives via terminal and frequency reference by remote terminal.

Following are programming parameters: --
-    [Access Level] LAC  to  [Expert]EPr
-    FR1 to Reference frequency via remote terminal
-    CHCF to Separate
Then it is possible to run ATV630 drives via terminal and frequency reference by remote terminal
Was this helpful?
What can we do to improve the information ?