Technical FAQs

Ask a Question

How to increase frequency reference up to 60 Hz on ATV310 drive.

Program the Max. frequency (308) to 60Hz 
Program High speed (512.2) to 60 Hz 

Then frequency reference will go up to 60 Hz.
Was this helpful?
What can we do to improve the information ?