Technical FAQs

Ask a Question

What are the identification of different buttons, LEDs and port on Hand-Held Test kit.

The identification of different buttons, LEDs and port on Hand-Held Test kit are given below:

A—Battery Compartment (five 9.0 V)
B—Short-circuit Trip LED (red)
C—Ground-fault Trip LED (red)
D—Ground-fault Inhibit LED (green)
E—Thermal-imaging Inhibit LED (green)
F—Trip Unit Power Supply LED (green)
G—Low Battery LED (amber)
H—Good Battery LED (green)
I— Trip Unit Test Cable 10-pin Port
J— 9 V Battery Test Button
K—Trip Unit Power Supply Button
L— Thermal-imaging Inhibit Button
M—Ground-fault Inhibit Button
N—Ground-fault Trip Button
O—Short-circuit Trip Button 
                                                          

 
Was this helpful?
What can we do to improve the information ?