Technical FAQs

Ask a Question

What are the specifications of battery for HHTK.

The Hand-held Test Kit uses five 9.0 V alkaline batteries (not supplied). Recommended battery is Panasonic Industrial Alkaline 9 V, part number 6AM-6PIX/1S, or equivalent. 

Note : Please do not use nickel metal hydride, NiCd, manganese or lithium batteries as damage can result to the internal circuitry of the Hand-held Test Kit.






 
Was this helpful?
What can we do to improve the information ?